Other Parts Discussed in Thread: SIMPLELINK-CC13X0-SDK, CC1310
Tool/software: TI-RTOS
Hello
I started to work with SimpleLink-CC13x0-SDK with CC1310-Launchpad Rev.1.3
My question is about, how can i combine different TI-RTOS examples under CC13x0-SDK.
In my application, i need both UART and PWM, it will start PWM, according the command coming from UART.
The "portable_CC1310_LAUNCHXL_tirtos_ccs" is good for start and working fine, and "pwmled_CC1310_LAUNCHXL_tirtos_ccs" is doing what i need.
I changed the "temperatureThread" in the portable_CC1310_LAUNCHXL_tirtos_ccs demo, with the "mainThread" in PWM Led example. But when i run the project, PWM is not working fine, it could
not open Board_PWM0.
pwm1 = PWM_open(Board_PWM0, ¶ms);
if (pwm1 == NULL) {
/* Board_PWM0 did not open */
while (1);
}
Can anyone help me?
BR,
Cagdas