This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200DK: 420-470MHz

Part Number: CC1200DK
Other Parts Discussed in Thread: CC1200, , CC1200EMK-420-470

Hello,

Few questions:

  1. Is CC1200 tunable to any frequencies between 420-470MHz?
  2. Are there any parameters in CC1200 transceiver that need calibration over 1-10 years using external RF source? Tx freq, Rx frequency, deviation etc? If so, is there an app note for calibration?
  3. US Railroads have license for 452 and 457 MHz. I need below eval kits parts? Are they available for purchase in US?

Name

Part#

Type

CC1200 Development Kit

CC1200DK

Development Kits

CC1200 Evaluation Module Kit 420-470 MHz

CC1200EMK-420-470

Daughter Cards

Regards,

David

  • Hi,

    1. Yes, CC1200 can be used in between 410MHz thru 475MHz
    2. Frequency accuracy depends upon the Crystal (40 MHz) being used. So, you need to refer to the Crystal data sheet.
    3. CC1200 DK is available to purchase in US
    4. CC1200 EM Kit 420-470MHz is not shippable to USA due to Export Restrictions.

    Thanks,
    PM