Tool/software: Code Composer Studio
Hello,
I have been using the sensor/collector example as a baseline for a project I am developing. While developing i noticed a drop in RSSI performance after network join. I see the same drop using just the examples. Using a spectrum analyzer while the sensors are trying to join a network I see average of -40 to -55 sitting in the same room, as soon as they connect that average rssi drops to around -90 to -100, obviously this is pretty terrible connection. I am just wondering is the channel that the sensor getting assigned to the cause of such a week connection? Has anyone else seen this? Also I tested these on custom boards and on launchpads saw nearly identical behavior. FYI i am using SDK 1.50 I was never able to get FH to work very well on 1.60.
Regards,
Jake