Tool/software: Code Composer Studio
Hello:
The default configuration for the sample projects is to split them over two projects. The instructions for combining them into one project is out of date (see here). However, I managed to get the project configured using the documentation as a rough guide. However, although there were no errors in the build setup, the build failed with an error about the symbol "DeviceFamily_XYZ" not being defined, despite the fact that the symbol is clearly defined in the build's Symbol settings.
The issue ended up being that the XDCTools section did not have the symbol defined. This shouldn't have happened and required a lot of time on my part to identify the root cause of the issue. Please submit a bug ticket to remove this line and have it reference the project build defines instead, or alternatively to include information in the #error message on how to resolve the issue using the XDCTools configuration page.
Thank you,
Michael