Hello,
I am not 100% this is the correct forum to ask this question. I am using the TI 15.4 with FH mode for my current project. I would like to use this stack to allow my sensors to continuously sample the ADC to read the out put of a Microphone circuit. I have modified the code and have everything working except that my power consumption is to high for any practical use. For my sensor controller task i used a modified version of the example Task Control, i removed the led and batt monitor from the code. Running the sensor stack with my adc task running i am using average 2.2 mA, if I build without ADC task i am using about .7 mA so my adc task is using roughly 1.5mA. I am looking for any suggestions on how to use the sensor controller to sample fairly frequently that will work in cadence with the 15.4 FH. The way the default is setup it does one reah periodically this will not really work for my application as I am trying to actively monitor sound levels. Any advice would be awesome, thanks in advance!
Regards,
Jake