Dear Sir/Madam,
I am using the CC1310 with the MCE_RFE_OVERRIDE(0,5,0,1,0,0) as I need Manchester encoding for legacy reasons.
I have found that the maximum frequency deviation is limited to 222 kHz. If 223 kHz is used, the deviation drops to 115 kHz.
This can be demonstrated using SmartRF studio 7. Use the override editor to set MCE_RFE_OVERRIDE(0,5,0,1,0,0).
I used a frequency of 914.321 MHz and a data rate of 20 KHz. There is no similar limit with MCE_RFE_OVERRIDE(0,4,0,1,0,0), but I can't use that as I need Manchester coding.
Is there any way I can use a higher deviation and keep the Manchester coding?
Regards,
Tony