Good day,
In my project, I need two devices: MASTER and SLAVE. MASTER should be capable of: 1) transmit to SLAVE 10 channels of uncompressed audio with highest fidelity and lowest latency possible; 2) receive from SLAVE 2 channels of uncompressed audio; 3) establish bidirectional UART port between the two devices. I am planning to use multiple CC8531/CC2590 configurations on a single PCB, as the space is crucially low.
Can you please advice, if these CC8531/CC2590 configurations could coexist in a closed to each other and if it would be too much interference between them for normal operation.
Thanks in advance.