Other Parts Discussed in Thread: REMOTI
Tool/software: Code Composer Studio
Hello All,
RemoTI Developer's Guide SWRU198D (fig. 4, page 12) shows point-to-point, point-to-multipoint, and multipoint-to-multipoint topologies, of which RC is only instantiated for point-to-point whereas Universal RC is for the multipoint scenarios. As far as CCS examples, what's the nuance differentiating the RC from the Universal RC?
My interest is in setting up and testing the Universal RC multipoint-to-multipoint topology to test DVD<--->STB communication, and so begs the further questions: are there any issues using Target Emulator to setup and test this topology: two Targets(DVD and STB) and one Originator (Universal RC)? If so, what other alternatives are there?
Please provide guidance, so I can test communication between DVD and STB.
Will I:
1) need to run two instances of Target Emulator (one each for DVD and STB) and Bind STB to DVD?
2) do I even need to first Bind STB and/or DVD to the Universal RC in order for DVD and STB to transfer data back and forth?
Thanks,
Manuel