Other Parts Discussed in Thread: CC2531, CC2650
hi i'm using CC2531 as ZNP and running Linux HA Gateway App on pi,
When i bind the ON/OFF Cluster Endpoint in ZED (cc2650) to ZC, i get the following msg:
Binding source selected
Sending bind command
binding source_address 0x124b00......40 endpoint 0x08
binding destination_address 0x124b00...fa endpoint 0x3
sent to NWK_MGR: len=36, cmd_id=26, subsystem=18
Raw= 24:00: ....
received from NMK_MGR: len=6, cmd_id=0, subsystem=114
Raw=06:00.....
Calling confirmation callback
comm_device_binding_entry_request_confirm: Received ZIGBEE_GENERIC_CNF
comm_device_binding_entry_request_confirm: Status SUCCESS.
received from NWK_MGR: len=21, cmd_id=27, subsystem=82
Raw:15:00:............
comm_device_binding_entry_rsp_ind : Received NWK_MGR_CMD_ID_T__NWK_SET_BINDING_ENTRY_RSP_IND
Bind/Unbind not successful (status=4)