This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2533: USART: UART and SPI (different alternatives) at the same time

Part Number: CC2533

Is it possible to use the same USART (0 or 1) with UART and SPI settings at the same time?

For example:

USART0 UART Alt. 1

RX P0.2

TX P0.3

and

USART0 SPI Alt. 2

MOSI P1.5

MISO P1.4

SCLK P1.3

SS P1.2

??