This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3000 Hangs After A Few UDP sendto Calls

In a loop, I am able to call UDP sendto a few times (sometimes once, sometimes up to six), but then it hangs on SimpleLinkWaitEvent(HCI_EVNT_SENDTO,...).  I am sending to a non-broadcast address on the same WiFi network.

Looking at previous threads on the same subject, the oldest threads suggest to upgrade to the latest driver and latest patch.  I am using the latest, which is now beyond those referred to in those older posts.  

    Host Driver Version:
       define DRIVER_VERSION_NUMBER   16
    PatchProgrammerMSP430FR5739-1.14.7.16.32

Why is this bug still existing if TI knew about it two versions ago?

The most recent post that I could find (from 2014) suggested to put a "considerable wait" after the first send.  I have put a 4 second wait in between all my sends since I started testing it, so that's not the solution.
Has anyone solved this for the last Host Driver and Patch?

2 Replies

  • No takers at all?

  • In reply to Jim Laskowski:

    Question for TI: Is TI's latest product development and support team(s) the same for the new WiFi product as the CC3000?  If so, I don't want to have anything to do with it.  CC3000 was a horrible product.  How can you fix a bug (UDP Hang) and then re-introduce it in later versions???  Have you heard of regression testing? 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.