Hello,
from Febrary 1,2015 all the Apps uploaded to the Apple Store must include 64 bit support. So, if i need to create a App that uses "libFTC_RELEASE.a" to send to Apple Store, i need a new version of it.
This is the Apple Message:
Starting February 1, 2015, new iOS apps uploaded to the App Store must include 64-bit support and be built with the iOS 8 SDK, included in Xcode 6 or later. To enable 64-bit in your project, we recommend using the default Xcode build setting of “Standard architectures” to build a single binary with both 32-bit and 64-bit code."
Unfortually "libFTC_RELEASE.a" library file, supports now only 32 bit.
Will be available the 32+64 bit version of it? if already exists, where i can download it?
thanks
Claudio