Hello,
Hopefully this is the right place to post, but I am having trouble using SmartConfig 1.1.
I have the Tiva C TM4C123GXL Launchpad with the CC3000 Booster pack and am trying to run the tcpEchoCC3000 example from the TI-RTOS v 1.21.00.09.
I've already patched the CC3000 successfully. When I run the tcp example, the readmefile says to push Button0 and it should put the device in discovery mode as indicated by LED0 (blue) blinking. This happens so I assume it is working.
However, I've tried connecting using the SmartConfig java app on the PC and the iOS app and the device never seems to connect.
I've:
*Set a Guest Network with no security.
*Guest network is 2.4GHz, bgn.
*PC is Windows 10, iOS is 8.1.2
*Example is in Section 2.2.6 from the SPRUHD4C—May 2013 TI-RTOS userguide.
*CCS v6.1.0.00104, XDCtools v3.25.4.88
*Start SmartConfig first, then run the device in debug. Then vice versa. Same in non-debug.
Not sure what else to do, any help is appreciated, thanks in advance.