while doing some miscellaneous testing with for Wi-Fi Local Server, I faced some issue . Everything looks fine, it communicate with two servers over Wi-Fi but I can't connect to Local Wi-Fi Server even message informing "WiFi server listening...".
I tried debug the code ( I was debugging with JLINK), where I found everything normal. In Firmware, Accept() to a new connection returns a handler (positive value) else it return -2 i.e. socket in progress every time. when any error on socket(), it returns -1.
In this scenario, return was -2 (SOCKET IN PROGRESS) is quite normal.
Next, I tried to capture the packet from client with expression "TCP" in wire shark, where I captured only SYNC packet from CLIENT. There is no response from CC3000. But I can capture ICMP packet for PING from both sides.
please help on this.