I have already executed "getting_started_with_wlan_ap" stater program given in the CC3100SDK_1.2.0 SDK using Code Composer Studio 6.1.3 and I am able to connect devices like mobile phones having wifi feature to CC3100 which is used as Access Point. With CC3100 I am using TM4C123GXL Launchpad.
Now I want to print the device information (like MAC, IP addrs etc) of the connected stations to Access Point in the serial terminal of Launchpad.So how can I query those information (like MAC address, IP address etc.) of the stations / devices connected to the Access Point.
I have seen "CC3100/CC3200 SimpleLink™ Wi-Fi® Internet-on-a-Chip User's Guide" . In this guide in Chapter 10 , I got something related to this under subsection in 10.4 "WLAN Parameters Query – API". Am I supposed to use this to query the device information or some other approaches I must adopt.
Please help me to find the solution.