This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CC3200: connectivity of SensorTag CC3200

Part Number: CC3200

Hello,

I have a problem to connect my SensorTag CC3200 with my PC (windows 7). Your CC3200-Getting_Started_Guide.pdf only describe how connect the CC3200 LaunchPad XL, but i can't find any information to connect the SensorTag with my PC directly. I want to get the gyroscope data on pc (as .csv or something like that), how can i do this?

Another problem is that one of my SensorTags CC3200 does not react of the reset (press both buttons 6 sec simultaneously). I had change his settings by his Url to WPA2 and passwort 123456, now i can not connect to this device by iPad and i cant reset the Sensortag, so i can't use it...

Can you help me please?

Best regards

Sarah

  • Hi Sarah,

    I don't believe you can pull data directly off of the SensorTag via PC connection.

    As for the SensorTag that will not reset, that sounds like there may be a hardware error with the reset pin. I would suggest contacting the TI Store for assistance in getting a replacement.

    Best regards,
    Sarah
  • Hello Sarah,

    The SensorTag Firmware (v1.003) exposes sensor data via HTTP, so you can browse to http://<sensortag_ip>/sensortag.html to read sensor data and configure the active devices/poll-rates/etc.

    You should see a page as follows :-

    ~roger

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.