Good day,
I am following the getting started tutorial that came with the CC3200 launchpad dev kit.
I have followed it line for line 3 times now.
Everything builds and works as suggested, except the last step where I need to debug.
I get the following error when I click debug:
The device is plugged in and powered up. The three lights are on the debugging interface.
When I click debug, the green led on the debugging flashes a few times then I get the error.
Jumpers are as suggested on the tutorial?
I see this in the console:
Cortex_M4_0: GEL Output: Memory Map Initialization Complete Cortex_M4_0: Error connecting to the target Cortex_M4_0: Error connecting to the target