With extensive testing we've determined that if sl_Stop is called while the nwp isn't running, it fails. We've also learned that sl_Start, if called while the nwp is already running, causes a memory leak (semaphores, etc call malloc). Is there an API call which will tell us if the simplelink is currently running, so we can protect calls to start/stop?