I have a new design using the CC3200. I can not get any out output from the 40MHz clock, 32KHz Clock or any of the DC regulators. I looked at pin 9 for example and the launch pad has about a volt output my boards has zero. All output are zero except the SPI_CL and its high.
I have Swapper crystal several time with 6 and 8.2 pf load cap, but no help.
Is there some lock up mode the device comes up in?
I have verified all pin connections and components. Everything looks OK, except the 3200 will not start.