I have 8 boards with CC3200 that I can not get to format or load the service pack with uniflash. I am using a launchpad with jumpers j6 & J7 removed. I have connected pin 3 RX to the GPIO_02(RX) and J7-3 TX to GPIO_01 TX of my board. I have also connected my board to the reset line of the launchpad. I have connected SOP2 high. I am also supplying the 3.3 v from the launchpad to my board. The 3.3 looks ok on a scope. I get the message ERROR:---- reading ACK signal failed ---- and after three tries it times out. Is my connection between my board and the launchpad correct?
Should I ever see a 40mhz clock on my boards? I do not.
This project is at a stopping point and critical!