This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 WiFi Direct (P2P) - Getting Recognition and Connection but no Data

Other Parts Discussed in Thread: CC3200

Hi - Trying to run the P2P Example with this WiFi Direct code from Github (https://github.com/ahmontero/wifi-direct-demoon a Galaxy S4. After successful recognition and connection, when trying to send the file, phone says "Unfortunately Wifi Direct Stopped Working". Pretty sure the code on both sides is correct - just not working together. I changed the Port number to match the 5001 in the CC3200. Maybe I'm missing some other changes(?).


Or is there another Android app example available that I should be using?

Thanks

D.K.