Using GCC via CCS 6.1.3
Debugger is XDS 100V2 JTAG Debug Probe(14 pin)
OS: FreeRTOS
SDK: 1.2.0
The problem is that we're calling ConfigureSimpleLinkToDefaultState() in our main task and it calls sl_Start( 0, 0, 0 ) which never returns. If we click the debugger's reset button at the top of CCS and try again it works. Each time we reset, it toggles between a working and non-working state. We only see the issue while using the debugger, but it's a constant nuisance to our development team.
From other posts, i see that we need to define "DISABLE_DEBUGGER_RECONNECT" but his did not solve my issue.
Please help us understand and resolve this issue.