Hi,
I find there are cc3220 files in TI web. I take cc3200 for two years and I want to change cc3220.
I have some questions about cc3220:
1. cc3200 can not link the 2.4G/5G router with iphone 5s(because SISO and MIMO) by one-key configuration, what about cc3220?
2.I designed cc3200 module by myself and it worked well. Could cc3220 replace cc3200 derectly without changing else devises?
3.I use IAR, how could I debug cc3220? There is not cc3220 in Options-General Options-Device.
4,I download SDK1.02.02.00 and install it, I can not find IAR project file and there is only makefile?
5. Where is SP of cc3220?
I study cc3220 by the first day and I am not familiar with it.
So, thanks.