Other Parts Discussed in Thread: CC3220S, UNIFLASH
I have a custom CC3220S board. It has both UART and JTAG headers.
I would like to connect only the JTAG header to the development PC ( via a XDS100v2 debug probe ) and
1) monitor UART while I debug;
2) flash new firmware using uniflash
Are these possible?
I have enabled "VCP" on both of my XDS100v2 channels and can see the corresponding USB serial ports are available from my "Device Manager". However, I cannot see any output from the serial ports while my program is running and uniflash also fails with a timeout error. When monitoring the serial ports, I have tried all available speed settings from 115200 down to 9600 8n1n.
Am I exceeding the capability of a JTAG connection?
I can, otherwise, debug OK with the JTAG connection and CCS7.