I can get data from the device, I can reset the device, but when I attempt an OAT upgrade to 1.003 Feb 22 2017 10:55:45 I'm met with a
OAT error -15
0 0 0
OAT err 0
error display on the watch module.
what am I doing wrong?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I can get data from the device, I can reset the device, but when I attempt an OAT upgrade to 1.003 Feb 22 2017 10:55:45 I'm met with a
OAT error -15
0 0 0
OAT err 0
error display on the watch module.
what am I doing wrong?
current firmware is 0.98a
batteries measure 2.9v
tried it on bench PSU set at 3.1v.
Same result.
When I try again I get
OAT run
and 15 seconds later the same error message.
Yours Simon Markham.
I have tried using the android update both from a phone and tablet.
Sorted now.In the end I had to use my sons iPhone. All of the android devices I tried failed with the same error.
I'm disappointed that the upgrade can only be done via OAT.