Other Parts Discussed in Thread: UNIFLASH, , CC3100
Hi, I am using the use the uniflash_3.4.1.00012_win32 to flash the CC3200 Launchpad for operation with the CC3200 Radio Tool. I have configured the CC3200 Launchpad jumpers position for uniflash operation and have completed the series of step from 'format' to 'Service Pack Programming'. I have loaded the binary file within the folder 'CC3200BoardApplication_Binary' for the Service Pack Programming as instructed by the CC31xx&CC32xx Radio Tool wiki page (processors.wiki.ti.com/index.php/CC31xx_%26_CC32xx_Radio_Tool#Introduction) but encountered the error message "ERROR: Incorrect bundle format. Please make sure you selected a valid service pack file. Operation cancelled."
When I tried to use the binary file from the CC3100_CC3200_ServicePack_1.0.1.11-2.9.0.0, there is no error during the 'Service Pack Programming' operation and the operation can be completed successfully. However, when I try to run the Radio Tool GUI with the CC3200 Launchpad board (with the board reset and jumpers correctly placed and connected to the RadioTooGUI), I encountered an error saying the firmware is incorrect.
Apparently, the radio tools binary files under the RadioToolGUI are needed for the RadioTool operation but cannot be programmed into the CC3200.
Please enlighten me how I can get the firmware correctly written to the CC3200 launchpad. If possible, please send me the binary file if you have a copy.
Any help in this matter is greatly appreciated! Have a nice day!