1) I have gone through the http server example and oob example, both are freeRTOS based. I want to change them in non-OS environment. How can I do this?
2) In both examples, How to bring the device as HTTP Server in AP -mode without having jumper on VCC-P58( No force AP jumper). So when user enters the SSID and password and priority on webpage the device will go into station mode and connect to the entered Wi-Fi router(as there is no jumper on VCC-P58)
Thanks.