I am using http server / oob example of cc3200 and the set up webpage of mysimplelink.net where the device comes as http server in AP mode first then user connects to it and goes to the webpage enter the Wi-Fi router connectivity credentials so the next time when the device is in station mode it should get connected to the router. I flashed the respective ucf and .bin files but every time of resetting the device, I have to remove/place the VCC-P58 jumper.
1) The http server example and oob example, both are freeRTOS based. I want to change them in non-OS environment. How can I do this?
2) In both examples, How to bring the device as HTTP Server in AP -mode without having jumper on VCC-P58( No force AP jumper). So when user enters the SSID and password and priority on webpage the device will go into station mode and connect to the entered Wi-Fi router(as there is no jumper on VCC-P58)
Thanks.