Part Number: CC3220
Tool/software: Linux
Dear support,
I porting code of my from cc3200 to cc3220, I using kit CC3220SF-LAUNCHXL but when I printff log have erros as below
I check mode = sl_Start(0, 0, 0) , mode = 1 , If true it must is 0
pls for Give me advice to port success
thanks
***START***
Voltage is 0 mV
RING PIN VALUE=0
Start RTC
Start TimerGPIOTask
HttpServerAppTask start
AKFRESH
GET_TIME: Begin
Start a P
> POWER DO2P main secWN!!!!!
CC3tion
200 version=02.02.10
Error [-2005] at line [254] in function [ReadFileFromDevice]
GET_APICannot read _VALUE 15
P2P ps_ip, eGET_API_HOSrror=0
T_NAME: api.cinatic.com
GET_MQTT_VALUE: 16
GET_MQTT_HOST_NAME: mqtt.cinatic.com
GET_NTP_VALUE: 12
GET_NTP_HOST_NAME: pool.ntp.org
GET_RMS_VALUE: 25
GET_RMS_HOST_NAME: relay-monitor.cinatic.com
GET_STUN_VALUE: 16
GET_STUN_HOST_NAME: stun.cinatic.com
Set cam default: flicker 50 UD 0 LR 0 brate 300 kbps framerate 15 resolution 360
HOST_NAME = api.cinatic.com
MODE_GET_CONFIG_FAIL, error=-10329
xxxxx___UNREGISTER
Network init start
lRetVal_ROLE_STA: 0
lRetVal_sl_Stop: 0
Failed to configure device to it's default state
Build Version 0.0.0.0.31.805306392.2.514.67174403.0.0.97.79
Switching to STA mode on application request
Error [-2032] at line [164] in function [Network_IF_WifiSetMode]
Error [-2032] at line [1090] in function [system_registration]