Other Parts Discussed in Thread: CC3220S, CC3220R
Hi,
Could you help understand the following statement from Figure 6.1 from datasheet ?
PIN 45 and 46: For CC3220S and CC3220R parts, leave pin 46 un-connected (DNP L5 and R8). Pin 45 can be used as GPIO_31 if a supply is provided on pin47
PIN 47: For CC3220S, CC3220R device connect to VBAT and add 0.1uF cap
Does it mean to disconnect both L5 and R8 ? If R8 is disconnected than there will be no power on pin47. Also, the above note for PIN 47 requires to add 0.1uF, however on the Figure it is 10uF (C20).
Could you re-phrase the above requirements?
Thanks,
David