Other Parts Discussed in Thread: UNIFLASH,
Hi,
We have a custom board housing cc3200 for connection over wifi. Currently our application requires that the wifi SSID and password and also a config text file having info like server IP and port number, ADC channel details etc to be flashed along with the main program via Uniflash. Current requirement is to use android app and input the details to cc3200 over wifi. Now I understand that there is the android app SimpleLink starter Pro for wifi provisioning. But using that we can only set the new SSID and password. Our application also requires putting the text file from android app only. We dont want to use uniflash each time the details like server IP and port in the config text changes. So can anyone direct me as to how to start working on this custom android app? I can not directly use the simplelink starter pro as it is, modifications are needed. It would be of great help if some reference source code is available.
Regards,
Sourajit