This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is AP mode possible, provided that the client connected (TCP socket) to the cc3200 device needs to make a "handshake" with the Internet servers via 3GSM (ppp connection will create a new interface)?
Are there any examples of embedding protocols in the existing stack of protocols cc3200? Is there any guidance on this issue?
What about the indirect support for PPP?
Hi,
Technically at socket layer (TCP) is possible do that what you want. You will need open TCP server at SimpleLink (WiFi) at AP mode. Connected client will send data to this TCP server. This data you will encode by your code to TCP/IP --> PPP --> HDLC and send to serial via your modem.
I am not aware about any implementation or tutorial for ppp at CC3200. But if you will want to know name of project which can be useful for you, I think it is LwIP. This open source project contains all necessary components. Porting to CC3200 will be up to you. I don't know how much effort will be required. Many years ago I implemented my own ppp stack including TCP/IP at ColdFire MCUs. Unfortunately I can't share this code.
Jan
Hello,
It is slightly embarrassing that in the AP mode in the AP's network there is no interface (gateway) looking into the Internet - as a restriction of this mode
(e2e.ti.com/.../433046 -
"...it does not have an ethernet host for other external connection to internet"). And in our case, after the PPP connection, such an interface appears. Perhaps something is wrong?
Hi,
CC32xx device are not designed for such applications, from this reason are advanced network features not supported. CC32xx devices are intended for low-power WiFi client applications. AP mode at CC32xx is generally used for provisioning.
In your case (discoursed above) this will not be a real gateway. Connection between networks will be at socket layer.
Jan