Part Number: LP-CC1352P7 Other Parts Discussed in Thread: WI-SUN Note: This guide assumes you have used the wfantund based solution with a TI Wi-SUN FAN Border Router. If not, please refer to the wfantund Readme and installation guide found here: https…
Part Number: CC2340R5
Dear users,
IAR Embedded Workbench users are recommend to use IAR 9.40.2 with F3 SDK 7.40.00.64. This information has not been properly reported in the release notes of the SDK.
Using previous IAR versions may lead to issue during…
Part Number: CC1352P7 Other Parts Discussed in Thread: CCSTUDIO , , SYSCONFIG
All,
Let this serve as a guide for getting Amazon Sidewalk SID demo up and running on the CC1352P7-1 Launchpad. Took me around 12 hours to get where I am comfortable building…
Part Number: CC2340R5
The purpose of these instructions are to detail how to merge/add multiple BLE profiles into a single project. The following is an example which uses the " data_stream_UART_over_BLE" as the base project and the "basic_ble_profiles…
Part Number: SENSOR-CONTROLLER-STUDIO
Sensor Controller Studio is used to write, test and debug code for the CC26xx/CC13xx Sensor Controller, enabling ultra-low power application design. The tool generates an interface driver consisting of C source files…
Part Number: WL1837MOD This new release includes firmware, driver, wpa_supplicant and hostapd updates.
The links to the repository of each component is as follows:
WL18xx firmware repo: https://git.ti.com/cgit/wilink8-wlan/wl18xx_fw/ --> master branc…
This guide shows how to use SDK Composer so the size of the SDK downloaded and installed is reduced.
This guide applies to the devices supported by the SimpleLink Low Power F2 SDK (CC13x1, CC13x2, CC13x4, CC26x1, CC26x2 and CC26x4) and SimpleLink Low Power…
Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: CC2340R5
The following details how to modify the uart2echo SDK example to enable the event Mask, and event Callback overrun on the LP-EM-CC2340R5.
Summary:
By implementing the following code…
Part Number: CC1312R7 Other Parts Discussed in Thread: SYSCONFIG , , UNIFLASH
Recently I had to go through a hard process of searching and trying to make first a different size program, then add serial tracing and last be able to encrypt it.
The idea of…
Part Number: CC2642R Other Parts Discussed in Thread: CC2652R , CC2652R7 , SYSCONFIG Hi,
Here are some steps to enable synchronization with a periodic advertising train on CC2642R, CC2652R or CC2652R7.
This guide assumes you are using the simple_central…