Hi
Does anyone know if the following configurations can be done with MCP CLI Tool?
- Place the radio in Continuous Transmit mode with pseudo-random modulated packets
- Place the radio in Continuous Waveform mode with non-modulated packets
- Place the radio in Continuous Receive mode and report successfully received packets
- Adjust the channel frequency to the low (1), mid (8), and high (13) bands (2.412 GHz, 2.447 GHz, and 2.472 GHz)
- Adjust the modulation of the radio
- Switch between B and G modes
Besides, does anyone know where can I find a good description of the different commands inside of the following menu Radio Debug --> Tx Debug-->Continues? I can see that they appear listed inside of the CLI Tool User's Guide but there is no explanation about which values or options can be assigned to each one of them. I'm talking about the following list:
Param 0 - Delay Param 1 - Rate Param 2 - Size Param 3 - Amount Param 4 - Power Param 5 - Seed Param 6 - Packet Mode Param 7 - DCF On/Off Param 8 - GI Param 9 - Preamble Param 10 - Type Param 11 - Scrambler Param 12 - Enable CLPC Param 13 - Sequence no. Mode Param 14 - Destination MAC Address
Regards
Igmar