• Resolved

WL1271 Bluetooth hciconfig hci0 inqparms pageparms

Hi,

I'm using the AM335x EVM with the ti-sdk-am335x-evm-05.07.00.00 SDK SD card, and I would like to change the inquiry and page timings.  But the commands don't appear to work.

E.g. the command "hciconfig hci0 inqparms 4096:180" should change the inquiry duty, but after executing the command, if I read back the values using "hciconfig hci0 inqparms", they have not changed to the new values.

root@am335x-evm:~# hciconfig hci0 -a
hci0: Type: BR/EDR Bus: UART
BD Address: 50:56:63:F7:AE:0C ACL MTU: 1021:4 SCO MTU: 180:4
UP RUNNING PSCAN ISCAN
RX bytes:8146 acl:134 sco:0 events:237 errors:0
TX bytes:4935 acl:152 sco:0 commands:84 errors:0
Features: 0xff 0xfe 0x2d 0xfe 0xdb 0xff 0x7b 0x87
Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3
Link policy: RSWITCH HOLD SNIFF
Link mode: SLAVE ACCEPT
bluetoothd[1506]: plugins/hciops.c:read_local_name_complete() hci0 status 0
bluetoothd[1506]: plugins/hciops.c:update_ext_inquiry_response() hci0
Name: 'XXXX'
Class: 0x4c0100
Service Classes: Rendering, Capturing, Telephony
Device Class: Computer, Uncategorized
HCI Version: 4.0 (0x6) Revision: 0x0
LMP Version: 4.0 (0x6) Subversion: 0x1f29
Manufacturer: Texas Instruments Inc. (13)

root@am335x-evm:~# hciconfig hci0 inqparms
hci0: Type: BR/EDR Bus: UART
BD Address: 50:56:63:F7:AE:0C ACL MTU: 1021:4 SCO MTU: 180:4
Inquiry interval: 4096 slots (2560.00 ms), window: 18 slots (11.25 ms)

root@am335x-evm:~# hciconfig hci0 pageparms
hci0: Type: BR/EDR Bus: UART
BD Address: 50:56:63:F7:AE:0C ACL MTU: 1021:4 SCO MTU: 180:4
Page interval: 2048 slots (1280.00 ms), window: 18 slots (11.25 ms)
root@am335x-evm:~#

root@am335x-evm:~# hciconfig hci0 inqparms 4096:180
root@am335x-evm:~# hciconfig hci0 inqparms
hci0: Type: BR/EDR Bus: UART
BD Address: 50:56:63:F7:AE:0C ACL MTU: 1021:4 SCO MTU: 180:4
Inquiry interval: 4096 slots (2560.00 ms), window: 18 slots (11.25 ms)
root@am335x-evm:~#

root@am335x-evm:~# bluetoothd -v
4.98

  • Hi,

    You are right if you run the below commands it does not change the intervals and also does not give an error.

    hciconfig hci0 inqparms 4096:180

    hciconfig hci0 pageparms 2048:180

    As the commands itself says window parameter first and then the interval as below:

    inqparms   [win:int]    Get/Set inquiry scan window and interval
    pageparms  [win:int]    Get/Set page scan window and interval 

    So please try the below, it worked for me.

    hciconfig hci0 inqparms 180: 4096

    hciconfig hci0 pageparms 180: 2048

     

    Thanks,

    Sundeep.

    Thanks for posting on TI E2E forum. We appreciate your feedback!
    Sundeep.

    ----------------------------------------------------------------------------------------------------- 
    ** Please click the Verify Answer button on this post if it answers your question. **

    Please visit our CC256x Forum Guidelines and FAQs

    Check out our CC256x Bluetooth Main Wiki page: http://processors.wiki.ti.com/index.php/CC256x

    Don't forget to check out our wiki page for lots of useful info:  Wireless Connectivity Platforms
    -----------------------------------------------------------------------------------------------------