Tool/software: Linux
Hi,
I have to checked the WLAN/BLE in continuous receiving mode and also tested it using random SOURCE/Destination MAC address.
WiFi continuous receiving : processors.wiki.ti.com/.../WL18xx_RX_Testing
BLE continuous receiving : http://processors.wiki.ti.com/index.php/WL18xx_Bluetopia_PM_Bluetooth_RF_Testing
But here in WiFi receiving mode, We have shown that to operate the WIFI in PLT mode , first need to down a wifi interface in board.
Because of that, in continuous rx test our device is not connected to any outside device, so what do we fill in source MAC address and Destination MAC address fields of continuous RX mode because
we do not know the source MAC at that time.
Due to above mentioned issue, we got PER value near about 1 which is not suiatable for FCC certification of the custom device
Thanks,
Ankit