Other Parts Discussed in Thread: WL1271,
Tool/software: Linux
Dear Sir,
My problem is after enable wifi by "connmanctl enable wifi", I can use other connmanctl commands to connect to AP, and also get correct IP address. But after that, the device can not ping to any other machine in the same network, even the gateway. I also can not ping it from my other host.
When I try to different iw or iwconfig command to set txpower or select channel, these command also not work. For example:
$ iw dev wlan0 set txpower fixed 18
command failed: Operation not supported (-95)
$ iwconfig wlan0 txpower 22
Error for wireless request "Set Tx Power" (8B26) :
SET failed on device wlan0 ; Invalid argument.
$ iwconfig wlan0 channel 2
Error for wireless request "Set Frequency" (8B04) :
SET failed on device wlan0 ; Invalid argument.
In my environment, we use:
Our linux is: Embedded Linux BSPs featuring the Yocto Project compatible Ångström distribution.
Kernel version: 3.14.52. Source from: Linux kernel: git.toradex.com/.../
CPU: iMX6 (current problem should not be caused by CPU).
I don't sure which component is missed in our environment. It also seems the code in drivers/net/wireless/ti/ folder is very old, seems old the the Wilink8 version 8.7, 8.6, 8.5 and 8.5. Can you give me some advice what I need to do next? Whether we just missed something or we need to integrate the new Wilink8 stuff into our code?
If possible, please tell us the possible technical support from Toronto of Canada side. My phone is: 1-306-203-6629.
Thanks,
Richard