Hi All,
I am currently working on wilink 8 (1837 module) MCP 8.5 linux driver. I am bit confused with the INI file (tiwlan_18xx.ini) parameter called Board Type under Phy Mac parameters whose value is set to 0x02.
Board_Type = 02 # EVB_18XX = 0; DVP_18XX = 1; HDK_18XX = 2; FPGA_18XX = 3; COM8_18XX = 4;
I have seen some of the forums mentioned the board type value should be 0x04. Can anyone tell me what is the difference between the values 0x02 and 0x04 and which one to use?
What will happen if i use the wrong board type value?
Looking forward for the replies.
Best Regards,
Prabhu