I am trying to do Tx testing with 5 GHz as outlined in processors.wiki.ti.com/.../WL18xx_TX_Testing
Below are details of the platform that I am using
- Host platform (Sitara EVM, BeagleBone, etc.)
- Freescale IMX6 based expansion board with integrated Wilink8
- Operating system (Linux, Android, etc.)
- Linux
- WiLink™ flavor (WL1837MOD, etc.)
- WL1837MOD
- Module vendor, if any (TI, Jorjin, Murata, etc.)
- TI
- WiLink™ firmware version (click here for more information)
- FRev 8.9.0.0.70
FRev 8.2.0.0.237
119381,46,release.c,PrintRevision,0|Firmware Revision (FRev) Rev 8.9.0.0.70
- FRev 8.9.0.0.70
The commands are:
/usr/bin/calibrator wlan0 plt power_mode on
/usr/bin/calibrator wlan0 wl18xx_plt tune_channel 165 1 0
/usr/bin/calibrator wlan0 wl18xx_plt set_tx_power 15000 0 1 165 0 2 0 0 0 0 0 0
/usr/bin/calibrator wlan0 wl18xx_plt start_tx 200000 11 1024 0 0 0 0 0 00:11:22:33:44:55 55:44:33:22:11:00 0
I do not get any transmissions with the above commands. The 802.11 sniffer draws a blank.Note that the antenna is selected as antenna #2. If I use antenna #1 with the following command:
/usr/bin/calibrator wlan0 wl18xx_plt set_tx_power 15000 0 1 165 0 1 0 0 0 0 0 0
with all other commands being same I get transmissions as expected. So the issue is when selecting antenna #2 for Tx testing.
Is there anything else that needs to be configured apart from the above to get the antenna #2 to work for Tx testing?