Other Parts Discussed in Thread: AM3357
Tool/software: Linux
We are encountering many, many instances of the following kernel log line.
2017-10-30 11:26:13.589 [288519.884275] wlcore: WARNING corrupted packet in RX: status: 0x3 len: 375
2017-10-30 11:26:13.455 [334447.241466] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 362
2017-10-30 11:26:13.379 [288557.482231] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 78
2017-10-30 11:26:13.229 [334856.475089] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 110
2017-10-30 11:26:13.159 [334484.578544] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 323
2017-10-30 11:26:12.999 [220153.902151] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 110
2017-10-30 11:26:12.999 [220153.901110] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 110
Some units log this line 500,000+ times per day.
I'm not sure what this line means, nor how to react to it. It does seem to correlate with particularly bad wifi performance on the WL1831MOD module, which is a critical customer issue for us.
Configuration:
WL1831MOD on AM3357
TI kernel 3.12.10
Kernel SHA: 7f280334068b7c875ade51f8f3921ab311f0c824
wlcore: driver version: R8.7_SP2-dirty
wlcore: PHY firmware version: Rev 8.2.0.0.240
wlcore: firmware booted (Rev 8.9.0.0.75)