Other Parts Discussed in Thread: WL1837
Tool/software: Linux
Hello everyone,
I would want to use the precise time synchronisation with a beaglebone black and a connectivity cape from Element14 using the WL1837 chip.
I did the following :
root@am335x-evm:/usr/share/wl18xx# ./wlconf-toggle-set.sh /lib/firmware/ti-connectivity/wl18xx-conf.bin sync 1 File: /lib/firmware/ti-connectivity/wl18xx-conf.bin Feature: sync Mode : 1 Enabling Feature: sync core.sg.params = 0x00000000, 0x00000000, 0x00000000, 0x00000001, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x0000000f, 0x0000001b, 0x00000011, 0x000000aa, 0x00000032, 0x00000064, 0x00000320, 0x000000c8, 0x000000c8, 0x00000000, 0x00000000, 0x00000000, 0x00000001, 0x00000000, 0x0000003c, 0x00001388, 0x000004b0, 0x000003e8, 0x00000001, 0x00000003, 0x00000006, 0x0000000a, 0x0000000a, 0x00000002, 0x00000005, 0x0000001e, 0x00000003, 0x0000000a, 0x00000002, 0x00000000, 0x00000019, 0x00000019, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000 core.sg.state = 0x01 root@am335x-evm:/usr/share/wl18xx# echo 100 > /sys/kernel/debug/ieee80211/phy0/wlcore/wl18xx/time_sync -sh: /sys/kernel/debug/ieee80211/phy0/wlcore/wl18xx/time_sync: Permission denied
Do you know if the "core.sg.params = 0x00000000" message is normal ?
I can't find any "time_sync" file in the "wl18xx" folder and naturally I have a "Permission denied" when I try the last command.
Did I miss something ?
Do you know how the sync function is working ? How can I verify it is actually working ?
Thanks a lot.
Best Regards
Will