Tool/software: TI-RTOS
Hi everyone,
I'm encountering some issues with CC2650, mounted on a custom board, communicating with a main MCU by SPI interface, where the CC2650 is the slave and the main micro is the master. I've implemented two tasks:
1) A task, that implements communication with the main MCU through SPI interface, that I've called SPI_TASK (SPI configured in Blocking mode without partial return)
2) A task, that implements communication with other RF devices, that I've called RF_TASK
I've seen that when I start to receive RF packets by posting rx command to M0 in RF_TASK, the SPI_transfer function returns with SPI_TRANSFER_CANCELED status.
If I do a RF_close the SPI_TRANSFER works correctly.
Thanks for clarifications