Tool/software: Linux
Hello,
We have WL1837Mod chip and using it on wifi phone. Roaming takes 10-30 second. With the same router and AP CISCO phone switch is very short. We event dont feel how it switches over.
I use sdk-linux-03.03.00.
1) I can see that rssi_treshhold is set -90 in main.c file ../net.wirless/wl18xx/main.c
2) We use wpa_supplicant with BGSCAN 5, -65, 30
3) Scanning is active. And hidden ssid is disabled. scan_ssid param is not used in the network node. The default should be 0 - disabled?
I am not sure if the problem is in rssi_treshold = - 90 in driver or bgscan params are not passed to driver.
Do you have what needs to be done to make roaming time less than 4 sec? This is for voice.
Also do you support 802.11r protocol?
Thank you
Grant