Hello everyone,
We are pleased to announce the release of our new ZigBee 3.0 compliant software stack, Z-Stack 3.0.0. This release is currently supported on our CC2530, CC2531, and CC2538 Wireless MCUs, with planned support for future Wireless MCU platforms.
Z-Stack 3.0 includes many enhancements over previous stack versions, including:
- Unification of many ZigBee application profiles into a single profile, providing seamless interoperability for all ZigBee 3.0 devices.
- The introduction of Base Device Behavior, which defines a common set of mechanisms for network commissioning that will be used by every device.
- Updated to the ZigBee PRO 2015 specification, which includes many security enhancements such as optional out-of-band key exchange methods, and other changes like enhanced child device management.
For a full list of changes introduced in the ZigBee 3.0 specification, please visit our wiki page:
http://processors.wiki.ti.com/index.php/What%27s_New_in_ZigBee_3.0
In addition, Z-Stack 3.0.0 will maintain backwards compatibility with all previous ZigBee application profiles by providing configuration options to allow legacy devices to connect to ZigBee 3.0 networks.
Z-Stack 3.0.0 also comes with new-and-improved sample applications. Building on the functionality provided with the ZigBee Home Automation sample applications, we have now added a comprehensive User Interface to the SmartRF05/SmartRF06 platforms that provide users with many run-time configuration options and give real-time data about the status of each device. More information about these sample applications can be found in the Z-Stack 3.0.0 Sample Application User's Guide, provided with the SDK.
As mentioned before, Z-Stack 3.0.0 is a ZigBee 3.0 compliant platform, and it has been certified against the ZigBee PRO 2015 specification, as seen here on the ZigBee Alliance webpage.
To download the new Z-Stack 3.0.0 SDK, please visit http://www.ti.com/tool/z-stack
Note: there is currently an issue with downloading Z-Stack 3.0.0 with Firefox. Please use Google Chrome or Internet Explorer to download Z-Stack 3.0.0.
Older Z-Stack releases have been moved to http://www.ti.com/tool/z-stack-archive