This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538DK: CC2538DK Quickstart guide in Z-Stack 3.0 Sample Application User's Guide does not work

Part Number: CC2538DK

I'm new to Zigbee and I'm using the SmartRF06 Evaluation Board with the cc2538 EM.  I've built the sample projects SampleLight and SampleSwitch from ZStack 3.0.0 without problem.  I flash a coordinator light to one board and an end device switch to the other board as per the guide.  The menu seems to function nominally when I go to commission the network on the coordinator which counts down from 180.  When I commision the end device the devices communicate back and forth as viewed form the packet sniffer. The commision screen displays "NS" and "NotOnNwk" disappears but nothing else happens.  The field "Id000 Srch 000/00" remains unchanged on the End Device while the Coordinator Id field counts down to 000.

I'm new to this so not having a working example is proving difficult.  Any help is appreciated.

Thanks, Colin