I am starting to put the openThread stack on the CC2538
About me - I have read the Thread v1.1.0 specification, I'm a former ZigBee developer and contributor to some of the ZigBee specs.
Plan:
I will be using a custom Schneider board that looks very much like the CC2538 Evaluation Module Kit except this has the cJTag port on it and the 6 pins for the UART on it.
Initially I've compiled the openThread Stack on a InstantContiki3.0 VMware image and created the hex file from the output .elf file on Linux.
I intend to use the SMARTRF06EBK-SmartRF06 Evaluation Board as my programmer and debugger using it's 10 pin compact JTag connection.
Questions:
Has anyone else already done this?
I would eventually like to move all my development to Windows. Has anyone compiled the openThread stack on windows? Where you able to import the project into any IDEs on Windows?
Has anyone gotten a debugger working and been able to set break points and step through the code?
Does anyone have traces of Thread traffic and a trace viewing program they would recommend?
Thanks
Jonathan