Support Path: /Product/Development and troubleshooting/
Dear TI,
I am working on a design using a CC2530 and its built in RF transceiver.
We are experiencing problems with spurious emission at 4.88 GHz. The operating frequency is 2.44 GHz, so I am inclined to believe that the TX oscillator is involved. The problem is present even when the transmitter is not used (i e the RF transceiver is enabled, and we are in RX mode).
Help with the following questions would be greatly appreciated.
1. Is the TX oscillator always on when the RF transceiver is enabled?
2. Is the TX oscillator set to the exact same frequency as the carrier frequency?
3. If this is a common issue, what solutions do you recommend?
BR,
Andreas