Dear TI,
According to our test today, we found the reason of below question is that the initialization time of function MAC_Init() call in the init time.
At room temperature, the initialization time of CC2538 is approx. 25~30ms.
When the ambient temp. is 105’C, the initialization time of CC2538 will be increased to up to 50ms.
And I used the zstack version is Z-Stack Home 1.2.2a.44539, can you show me what the function MAC_Init() do, because it sometime in room temperature is only execute 3ms, but sometime in high temperature it executes more than 25ms.
We don’t have the source code of this function, so please show me any information is appreciated.
Because we are caring about the current consuming and if too long time initialization is very bad news for us.
So can you show me why the MAC_Init() 's execution time is not stable?
BR,