This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-Stack 3.0.1 (CC2530/CC2538) is now available!

Other Parts Discussed in Thread: Z-STACK

Hi everyone,

Z-Stack 3.0.1 is now available to download on TI.com at the link below. This SDK is a mainly a maintenance release for Z-Stack 3.0.0, no major new features were added but many bug fixes have been included. Full changes are available in the release notes included with the SDK. Since there were no major changes, migrating from Z-Stack 3.0.0 to 3.0.1 should be as simple as moving your IAR project files (for example, your SampleLight project folder) from the old SDK to the new SDK.

Note that the IAR workspaces in this release have been updated to use a newer versions of IAR IDE.The version numbers for IAR ARM and 8051 are available in the Z-Stack 3.0.1 release notes.

Warning: There is a known issue with IAR ARM 8.11.2 that causes build to fail for most projects. We are currently working with IAR to resolve this, for now please make sure you are using IAR 8.11.1, all projects were tested using this version before the SDK release.

Download available here:

http://www.ti.com/tool/z-stack

Z-Stack 3.0.0 should now be considered deprecated, it has been moved to:

http://www.ti.com/tool/z-stack-archive

Known issues and Proposed Fixes are documented here:

http://processors.wiki.ti.com/index.php/Zigbee_Known_Issues_and_Proposed_Fixes