hi
till now i have Zigbee device that is ZNP and use as coordinator
and i have Zigbee device that i want use mcu 8051 in it as Router
in sample app, i add these lines as well as similar in znp to set up a coordinator
bdb_setChannelAttribute(true,0x2000); bdb_setChannelAttribute(false,0x0000); bdb_initialize (); bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING);
in other zigbee that use znp i rcved this
FEh 0Ch 45h CAh 6Fh 1Ch 94h 60h 6Bh 0Fh 00h 4Bh 12h 00h 00h 00h 39h
according to document
and what my 8051 MCU return is this:
DEV_END_DEVICE_UNAUTH Joined but not yet authenticated by trust center
where should i authenticate ?how can i authenticate?
what is the function?
should i authenticate in ZNP that is Coordinator or in 8051 that is router?